Configure Onboard I/O
The procedure to define the local I/Os of the AKD drive is very similar to the one for I/O slices, with these exceptions:
- Channel column also contains in brackets the connector and pin number.
- PLC variable selection applies to digital inputs and analog inputs and outputs.
- See Map I/O from the Project Explorer for more information.